This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020EVM-487: BG96 GPRS/NB-IoT power supply

Part Number: TPS63020EVM-487
Other Parts Discussed in Thread: TPS63020, TPS61022, TPS61020

Good morning,

I'm using the evaluation board of the TPS63020 in order to power supply the BG96 modem by Quectel. I have setup the evaluation board (change R1) in order to have 4.2V at the output.

Input voltage for the evaluation board is 3.3V.

TPS63020 is working fine when BG96 is working in Nb-IoT mode (less power consumption) but it is not able to work well when BG96 is set to work at GPRS mode: in GPRS mode, TPS63020 is delivering 4.2V but important 2V down-spikes at this output are noticed when modem is trying to work. I have tested this with 3V3 voltage coming even from a 2A power supply, but result is the same (first, the 3V3 were delivered from my circuit).

Do you have any suggestion to cope with this?

All the best,

Dani