Other Parts Discussed in Thread: TPS54540
I'm having start up problems with the TPS54626. I used Webench to design the switcher supply. The layout closely resembles that recommended in the datasheet. The load has a pretty big range. It ranges from 10mA to 3.5A. I just had 4 prototype boards built. All exhibit the same issue but two of them require a higher load current to see the issue. I believe that my issue is an output undervoltage lockout problem (I don't know why because I'm operating the chip within its parameters). The chip latches when this condition occurs which is really bad. I monitored the feedback voltage (Vfb) and the Soft Start voltage. The feedback voltage seems to ramp up to around 530mV and then slowly climb towards the typical 765mV level. When the board fails it simply shuts down at about 1.7 times the soft start time which is why I think it is the output undervoltage lockout kicking in. Note, if I reset the switcher via its enable pin then it comes right up. After an enable pin reset, the feedback voltage ramps straight up to the 765mV (it doesn't go to the 530mV and then slowly ramp to 765mV). What should I look at to try and fix this issue?
Here is an o'scope capture of the voltages (Yellow = Vfb, Blue = Soft Start pin) when it fails:
Here is an o'scope capture of the voltages (Yellow = Vfb, Blue = Soft Start pin) when I reset the switcher using its enable pin (note no power cycle):
Here is an o'scope capture of the voltages (Yellow = Vfb, Blue = Soft Start pin) when the board doesn't fail (lighter load):
Note, the bottom horizontal cursor is at 530mV and the top horizontal cursor is at 770mV.
I appreciate any help!!