Hello,
We have been experiencing some issue from bq20z95 device bases BMS. The findings include
1. After voltage calibration, the voltage measurement reading of bq20z95 did take 1-2min to settle down and stable.
2. Our ATE followed Ti "SLUA355B-August 2005-Revised January 2010" instruction Section5"Calibration" to process CC Offset Cal, while no load connects to Pack terminal. After calibration we did see CC Offset period of time jump from 0mA to 7mA then fall back to 0mA from some device, other constant 5mA error while no load connected. We tried to use bqEasy instead of our ATE to confirm the finding and also got 5mA-7mA error after CC Offset even Board Offset calibration through bqEasy.
Question:
1. Regarding Voltage settling time: why does device operate with so long settling time? Is any way from hardware or FG configuration could eliminate such operation behavior from FG?
2. Regarding CC Offset error: why the CC-Offset calibration could not eliminate the error to 0mA, Board Offset also seemed not help? Is this error associates with FG configuration(dead band) or bad performance
by digit filter?
Thanks,
Jenny