Hello team.
We would like to make sure that TPS92692 is being used within a safe temperature range.
To do so, we need to know the power consumption of the TPS92692, but we can't find anything related to the datasheet.
Could you tell me how to calculate the power consumption or the recommended package temperature range of TPS92692?
- VIN=24
-VOUT=28~34V
-Imax=6.0A
-Fsw=200kHz