This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best Solution to charge lithium battery pack

Other Parts Discussed in Thread: BQ24650

My customer has the following spec for their battery and needs to have a charging system that supports this type of battery configuration, probably 6-series and N-parallel (TBD):

 

Voltage  : 16 V - 28 V range

Capacity : ~110 Watt-hours

Current  : 10 A continuous, 12 A peak

Chemistry: Lithium

 

They have a BQ28210EVM with a matching BQ gas gauge EVM, but is something more appropriate now for this application?