This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Questions about BQ25156

Other Parts Discussed in Thread: BQ25156

Our project FM8+ Morgan is using to add attached PMIC BQ25156 and have below questions want to consult you.

We found that the input current of BQ25156 IN pin is set to 400mA (ILIM: 101), but in fact the input current can only be up to 130mA, no matter changing the upper limit of the input current of ILIMCTRL Register (0x19), the input current is still only 130mA.