The TPS610994YFFR input is 3.0V (from Alkaline battery) with 3.3V output design. When that boost converter is exposed to sunlight, the output goes up to 3.9V which exceeds the absolute maximum ratings for other devices. Please see the schematic below and recommend to us how to resolve the sunlight sensitive issue. We need the output to stay at 3.3V in the presence of sunlight.