This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Are there any buck-regulator controllers (external MOSFET) that can do 100% duty cycle?

Other Parts Discussed in Thread: LM5085, TPS40200

I'm looking for a buck-regulator controller that can do 100% duty cycle. This means that when the input voltage drops too low, the high-side FET permanently turns on and becomes a passthrough. I also need to be able to synchronize with an external clock.

Some of the switching regulators with integrated FETs can do 100% duty, but none of them have a sufficiently low Rds(on) for my needs. If I could use a controller instead, then I could choose a suitable FET that meets my needs.