Dear Sir,
I am searching for a charger with FG inside.
The below function is nice to have. BQ25895 could meet, but it doesn't have FG inside.
Would you help me check if TI has an available part?
Application:
1.with Power path, and current to system > 3A, charge current to battery > 1A
2.Need able to monitor NTC on battery pack side //NTC -> TH05-4H104FR ,100KΩ±1%,B=4360K
3. Need able to enter ship mode
4. able to support QC/PD adapter (Nice to have)
Thank you,
Hugo