Hello,
I believe that a single channel controller (e.g. lm74700-q1) cannot prevent some (transient) cross conduction between the 2 channels.
This is because it takes some time (or some reverse current) to turn OFF the MOSFET that was initially ON.
My application cannot have this type of cross conduction behavior.
A solution would be to use a dual and/or triple channel controller.
A 2 or 3 channel controller can implement a "break before make" scheme in order to prevent cross conduction.
Do you have any dual and/or triple channel ideal diode (/ power ORing) controller ?
My application in short:
- 2 and 3 channels ideal diode / power ORing
- VDC max = +14.5V
- IDC max = 25A
- N channel MOSFETs preferred