Other Parts Discussed in Thread: BQSTUDIO, BQ34Z100-G1, BQ40Z50
Hi Expert,
Will need your support to know how to design the BQ4050 to support one cell setting.
Condition:
--System only connect to One individual 12.8V battery directly (4 cells in series inside).System not connect to individual 4 cell separately
--LiFePo4
--Consider the BQ4050 for system side gauge
Now We connect this individual 12.8V battery to BQ4050 EVM directly at VC1,then short the VC1~VC4 together. Since we think this is one cell for BQ4050.And system can not connect to individual 4 cell separately.
Then using the bqstudio to communicate with EVM and this individual 12.8V battery.
But now we see the voltage of CELL 1 show 0V from bqstudio.
But use one 4V battery to instead of the 12.8V battery with same configuration.The cell1 reported the voltage correctly.
We try to increase the Safety Cell Overvoltage and Safety Cell Overvoltage setting to 15V in case the OVP is triggered, but still not work.
So will need you to advise us how to configure the EVM and setting the bqstudio.
If possible, can you also run the bqstudio with this conditions and forward the log files to us.
Then we follow your setting directly.
Thanks
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E-Mail:Eric.Lai@ti.com