Other Parts Discussed in Thread: BQ25895, BQ27510, BQSTUDIO, EV2400
Hello,
I have GPOUT wired to the CE pin on a BQ25895 with a pull-up. All I want it to do is disable charging when the battery is too hot or cold, but it seems like right now it just always leaves GPOUT high. Do I have this configured properly for this operation? I just left the registers as their defaults in the golden image. PFC_CFG[1:0] = 01
Honestly the manual is not very clear on this because it talks about the GPOUT pin in so many ways. It is confusing because you set the PFC_CFG which suggests it controls GP_OUT but then I don't know what BAT_FN and GPOUT_INT should be set t.o If you want it control GP based on thermistor temperature do you have to tell it to use BAT_GD functionality? It isn't clear how the PFC_CFG config relates to GPOUT_INT and BAT_FN
I also find it disappointing that there is no explanation as to what goes into determining "Battery Good (BAT_GD)" so hopefully someone could elaborate on that.
Thanks