This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: if the BQ27220 can be used in handset device

Part Number: BQ27220

When the battery has been used for 1% and shut down ,the BQ27220 's parameters only hold on for 60 hours.

If we reconfigure the  BQ27220 's parameters,we must wait for completing a full charge and a full discharge.

It need maybe six hours. There's no handset device that needs to be used like this。