This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6ch 300mA LED driver selection

Other Parts Discussed in Thread: TPS92200

Hi,

I am considering an LED driver circuit with the following specifications.
Is there an LED driver that meets the specifications?
For example, I think it is possible to use a step-down converter to reduce the voltage from 24V to 7V and then apply a voltage of 7V to the LED driver.
I've been thinking a lot, but I can't find a good idea.

(specification)
VIN: 24V
VLED: About 6V (LED voltage is about 3V in 2 series)
LED current: 300mA
Number of LED strings: 6ch
DIM control each channel with PWM signal, but register setting such as I2C is not possible

Best regards,