Part Number: TPS51200-EP
Other Parts Discussed in Thread: TPS51200-Q1, TPS51200
Hello,
On the datasheet of TPS51200-EP, the refout tolerance to refin is +/-15mV @ +/-10mA.
On the datasheet of TPS51200-Q1, the refout tolerance to refin is +/-15mV @ +/-10mA and +/-12mV @ +/-1mA..
On the datasheet of TPS51200, the refout tolerance to refin is +/-12mV @ +/-1mA.
We are using the EP version for DDR4 so we need to have less than +/-12 mV on Refout. The TPS51200-EP is given for DDR4.
Is it the datasheet which is not up to date ? Can we use the number given in the TPS51200 datasheet for the EP version?
Thanks