We are using UCC256402 for half bridge LLC converter, where Vhv = 150V.
According to datasheet, it is mentioned that Vcc supply voltage range is Min: 13V, Nom: 15V, Max: 26V in recommended operating condition table. But IC didn't work when provided 24V at Vcc pin, then there is another table which mentions - VCCStartSelf: min :25V, TYP: 26V, Max: 28V , Which is quite contradictory to the earlier statement.
So the question is if IC doesn't work below 26V then what is the meaning of recommended operating condition ?
When we reduce (after start up) Vcc voltage from 26V to even 24V, IC stops generating switching waveforms. IC always needs 26V supply to Vcc pin in order to make it work.