Hi Colleagues,
Please check if i got this correctly:
Abs max of REGIN is defined by:
The Maximum value is: "The minimum of VSS+6 or VBAT+0.3"
Vss+6 is typicall 6V
VBAT is >60V with 16 cells.
That means the absolute maximum of the REGIN pin is 6V in this case. Can you clarify if i read this correctly and there is no voltage > than 6V (from VSS) allowed?
is this guaranteed by the pre-regulator transistor via BREG?