Other Parts Discussed in Thread: , TPS2121
Hello,
I just have an inquiry with regards to a possible addition of a USB-C port to charge my 4.2V Lipo battery at 5V. I followed the layout and schematic provided in the BQ24650EVM-639 with a few changes to match my solar panel's 6.3V MPPT voltage and and 4.2 V 1 cell battery. My issue is that I sometimes require a more stable voltage source during times of poor solar exposure.
I have noticed that Voltaic systems have designed their own version of a MPPT solar charger with the BQ24650 chip which includes a micro usb to charge at 5V by turning a knob potentiometer on the board itself to change the programmed MPPT voltage. Is it absolutely necessary to always make this change when connecting a 5V source to charge the battery? Also, with regards to the voltaic system's board, the USB should only be connected when the solar panel is disconnected and while that is fine, would there be a way for the chip to detect when charging from the USB source and switch to that instead of the solar panel voltage?
I have attached my schematic of the BQ24650 for the time being and was curious to see if there would be any issue if I connected a USB-C's voltage in pin at the Vin point between the D1 and TRS2 diodes found at the top of the schematic shown below.
Your feedback is greatly appreciated.
Thank you.