Other Parts Discussed in Thread: UCC28951
provide circuit diagram SMPS used SG2524 for 2K Watt power using external Mosfet or IGBT , input 200V to 400V DC out put +24V/40A and -24V/40A dual power required
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gangaram,
TI does not have a circuit design for the SG2524 in a 2kW system that matches your specification.
Normally customers use the UCC28951 in this type of application, 
You can find a number of reference designs using the UCC28951 device at 
Regards
Peter