What should be done with the d+/d- pins when the input isn't a usb source?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Justin,
The D+/D- lines can be left floating to detect unknown adapter and set IINDPM to 3.0A or shorted together to set IINDPM to 1.5A. Check in mind that with the ILIM_HIZ pin enabled, the resistor from ILIM_HIZ to gnd clamps the input current limit regardless of what is autodetected.
Regards,
Jeff