This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM3405: LM3405AXMKX/NOPB----We are not able to generate design form webench tool

Part Number: LM3405


Tool/software: WEBENCH® Design Tools

Hello Team ,

We are planing to Use LM3405AXMKX/NOPB as IR Buck but we are not able to generate the design for this 

Below are operating condition :

1.No of IR LED : 2

2.IR LED Forward Voltage : Min 1.2V and MAX 1.7V

3.Current Setting : 1A  or 500mA

4. Buck Input Voltage : 3V3

Please help to generate this design .

Thanks ,

Shubham