Other Parts Discussed in Thread: TPS61023
Hello
I hope someone help me with power rail design.
Because of the space and ext.price of power parts, I need to simplify and find new solution.
I designed the power rail with BQ25616 + TPS61023 + PMIC
The Powers required are 5V, 3.3V x 2, and 2.8V. and battery is 1-Cell Lipo.
PMIC is used to supply 3.3V x 2 EA and 2.8V.
TPS61023 is to supply 5V to NFC reader and PMIC.
Is there good chip in TI to cover BQ25616 + TPS61023 ?
Is there good chip in TI to cover BQ25616 + TPS61023 + PMIC ?