This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: bq27426 Questions.

Part Number: BQ27426

Hi Sir,

Pls kindly help for bq27426 questions as below, thanks.

Is it means need to try again CFGUPDATE or it means gauge initial fail If MCU read gauge FW VER not 0202?

   W: AA 00 02 00

   C: AA 00 02 02

5.1.3 FW_VERSION: 0x0002

Instructs the fuel gauge to return the firmware version to addresses 0x00 and 0x01.

need/no need to do CFGUPDATE can confirm by FW VER? or ITPOR of FLAG REG?

ITPOR = Indicates a POR or RESET subcommand has occurred. If set, this bit generally indicates that the RAM

configuration registers have been reset to default values and the host should reload the configuration

parameters using the CONFIG UPDATE mode. This bit is cleared after the SOFT_RESET subcommand is received.

Thanks, Ian.