Other Parts Discussed in Thread: OPA855, , TPS7A39, TPS730, LP2992
Hello together,
I would like to supply the operational amplifier OPA855 with ±2.5 V. I wanted to use two LDOs (positive and negative separated).There is a switching regulator before the LDOs. The output voltage of the switching regulator is ±3.3 V. Using LDOs I bring this voltage to ±2.5 V. I have chosen a negative liner regulator.
The series is TPS723. Now I need a positive one from the same series. Can you suggest one that I can combine with TPS723 to power the OPA855?
Kind Regards
Selvedin Hodzic