Other Parts Discussed in Thread: TPS23758, PMP40514, , TPS23730EVM-093
Today I learned that there is a difference between forward and flyback transformer and inductor requirements. Would would have anticipated such a thing?!
I have another TPS23758 in the works so hopefully that's "so simple" that this thread isn't urgent. But I would still like to understand what I'm doing since I have a pile of parts which would be good to use at some point.
I started off with the schematic from the PMP40514 (A secondary side forward "looking" converter). I picked the Coilcraft POE13P-50L (A flyback transformer)... at that time it said transformer for the TPS23756, so I figured I was good :)
https://www.coilcraft.com/en-us/products/transformers/power-transformers/power-over-ethernet/poexxp/
I noticed in another post the following quote:
For your reference, I would highly encourage the customer to follow the PMP405414 design. It uses the TPS23756 and is an active clamp forward with 12V output. Since it is a proven design, I see no reason not to directly copy it.
But at the bottom of the PMP40514 Schematic it is titled:
Project Title: Class 3 Isolated High-Efficiency Active Clamp Flyback Converter for PoE PD Reference Design
So me being completely clueless that I was clueless... suddenly started thinking... hey my PMP40514 output has a single diode and needed a big inductor (330nH)... certainly looks like a forward converter.
(I even tried the 10uH SER1360-103KL for the TPS23756-EVM Flyback and it DOES NOT WORK! (as you know... and I didn't))
So... why does the flyback transformer work for my forward circuit? I read that the flyback uses the transformer like an inductor to hold energy, but a forward doesn't use the transformer that way (which is why the big inductor value is needed later).
Is my crazy flyback transformer storing energy and delivering it out of phase or something insane like that?
Is my circuit going to suddenly stop working (I'm drawing at least 10W out of it with no issue.. my electric load is on order! bear with me while I order the world!.. I just got my bode meter today!)
Is my circuit perhaps just a little inefficient? Or am I in for a big EMI trap when I try to get certified?
Being that the PDF says PMP40514 is a flyback, but... the secondary looks like a forward... are we in some middle ground that... I don't even know how to interpret where I am.
The crazy thing is I am not smart enough to pick this transformer myself, and I swear that coilcraft just a few months ago was promoting the POE13P-50L for the TPS23756... but there's no sign any more.. am I losing my mind? Now that I look, it's clearly not listed in any reference design.
Anyways, if this monster I've created is no good... it's fine. I just want to know that if this POE13-50L flyback transformer shouldn't be used in the PMP40514 forward secondary, to know now... rather than thousands gobs of money later.
If you know, please share :) If not, no big deal. :) I'm just trying to determine the "right thing to do" with this pile of TPS23756 and POE13-50L parts next to me :) -- it's a long story
Thanks!