Other Parts Discussed in Thread: LM5088, UCC5304
Hi all,
Please answer the question on following URL;
Regards,
ACGUY
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm not sure the LM5088 can be used reliably for high voltage conversion like that. Let me check.
What's the TINA error you get?
-Orlando
ACGUY,
I had to replace your MOSFET and diode because I did not have the libraries.
When I test with 100V components I first got a convergence issue with TINA.
Is that the issue you're seeing?
I can fix the convergence issue by going to "Analysis-> Set Analysis Parameters" and increasing the relative error tolerance like below.
Hope this helps,
-Orlando
Hello Orlando,
Thank you for reply. However, I want to get really answer is for devices combination for DC/DC.
My idea is using an isolated gate driver as a boot strap for turn ON high side FET.
Could you discuss the circuit configuration with me? Or Could you introduce someone who can discuss?
Best regards,
ACGUY
AC Guy,
The feedback I received from the UCC5304 team was the bootstrap-capacitor may have trouble charging or keeping charged at startup with a non-synchronous topology. Their recommendation is to use a synchronous configuration as shown in the UCC5304 datasheet.
Perhaps you could pull switching node to GND to charge bootcap, but you risk shoot-though of the 400V if error or failure.
Another recommendation is to use a PFET with a non-synchronous solution like below.
Hope this helps,
-Orlando