Hi,
The query thread "PTR08060W failures - looking for hints and ideas" which is already posted in TI forum is related to my query as well.
We are having an issue with PTR08060W. The output voltage of the module appears same as the input voltage (12V in our case).
Want to know what is the resolve steps suggested for the above thread. It is in locked state now.
To brief about our design, we feed 12V input to PTR08060W and generate 1.5V at the output.
When we measure the output voltage, it is 12V (Same as Input voltage).
Here are the details required about our design.
Inhibit pin is driven by the tri-state buffer with No pull ups on the line. Input of the Tri-state buffer is at ground level.
One 22uF ceramic capacitor (GRM21BR60J226ME39L) is used at the output and 2 Nos Tantalum capacitor (T530Y477M006ATE005) 470uF is used at the output. Their ESR value is 5m ohm @100kHz.
Please help to resolve the issue at the earliest possible as we are struck in testing.
If you need any other details, kindly let us know.
Thanks & Regards,
Sathiya Seelan Sekar