This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24193: charge timer

Part Number: BQ24193
Other Parts Discussed in Thread: BQ27531-G1

Hello

I want to know all case that REG09[5:4] goes 11.

・Chage timer expire( set from REG05)

・1 hour has passed in the state of BATLOWV

Are there any other cases?
I set it up for 12 hours from bq27531-g1, but  timer expiration occurred after 1 and a half hours from charging start
Y.Kuramoto.

  • Kuramoto,

    If the charger device is in DPM regulation or thermal regulation during charging, the actual charging current will be less than the programmed value. In this case, termination is temporarily disabled and the charging safety timer is counted at half the clock rate.

    Referring to 8.3.3.6 Charging Safety Timer on the d/s:

    The following actions restart the safety timer: • At the beginning of a new charging cycle • Toggle the CE pin HIGH to LOW to HIGH (charge enable) • Write REG01[5:4] from 00 to 01 (charge enable) • Write REG05[3] from 0 to 1 (safety timer enable) • Write REG01[7] to 1 (software reset)

    During input voltage/current regulation or thermal regulation, the safety timer counts at half clock rate since the actual charge current is likely to be below the register setting. For example, if the charger is in input current regulation (IINDPM) throughout the whole charging cycle, and the safety time is set to 5 hours, the safety timer will expire in 10 hours. This feature can be disabled by writing 0 to REG07[6].

    Thanks,

    Ning.

  • Hallo,

    How about below?

    --

    I want to know all case that REG09[5:4] goes 11.

    ・Chage timer expire( set from REG05)

    ・1 hour has passed in the state of BATLOWV

    Are there any other cases?
    --
    If REG09[5:4] goes 11,can I think either of the above two cases?
    Y.Kuramoto
  • Kuramoto,

    Referring to 8.3.3.6 Charging Safety Timer on the d/s, In default mode, the device keeps charging the battery with 5-hour fast charging safety timer regardless of REG05[2:1] default value.

    Thanks,

    Ning.