Other Parts Discussed in Thread: EV2400, BQSTUDIO
Hi,
I'd like to use BQ27441-G1 in a system where I have multiple I2C devices on the same bus as this fuel gauge connected to a host micro-controller. I have a few questions regarding correct practice of hardware implementation when it comes to high volume manufacturing:
1- I understand we can configure the fuel gauge using BQStudio. What's the correct practice for providing flexibility of using BQStudio in my schematics? Should I just simply put pin-headers for tapping into I2C line and connect EV2400 externally using jumper wires? Is BQStudio used in production stage or there's a work-around using host micro-controller?
2- A LiPo battery is permanently connected to the system and because of the nature of our design the load cannot be disconnected from the fuel gauge. How can we perform the board offset calibration properly? There's indeed a power button in the system but there are other components before the switch which doesn't let the current flow through BQ27441-G1 sense resistor to be absolute zero. In prototyping stage there's definitely a work around for this to disconnect the load (i.e. using jumper). However, I was wondering if we can bypass this stage in production by using same board offset calibration value from prototyping stage.
3- Since the fuel gauge already has temperature readings, we would like to use that data in other part of our software logic for different purpose. Does BQ27441-G1 do the temperature measurement using the 10k pulled-down resistor (thermistor) connected to pin BIN? Or it has its own internal temperature sensor?
Note: We are planning to permanently pull down pin BIN since the battery is embedded in the device.
Thanks,