This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC21520-Q1: Revision History

Genius 4840 points
Part Number: UCC21520-Q1

I found following description in page2  Revision History.

• Added cross reference to table note 1 .................................................................................................................................. 5

But I can't find cross reference in page 5. Please let me knoe what means this description.

  • Hi, Kura,

    Previously, the footnote #1 was:

    (1) Stresses beyond those listed under Absolute Maximum Ratings may cause permanent damage to the device. These are stress ratings only, which do not imply functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability.

    In the revised datasheet, it is now:

    (1) Stresses beyond those listed under Absolute Maximum Ratings may cause permanent damage to the device. These are stress ratings only, which do not imply functional operation of the device at these or any other conditions beyond those indicated under Recommended Operating Conditions. Exposure to absolute-maximum-rated conditions for extended periods may affect device reliability. See Application and Implementation for more information on the typical application and how to avoid device overstress.

    Let us know if you have further questions. If this answered your question, please press the Green button.