Other Parts Discussed in Thread: LP2992,
Hello together,
I am using two switching regulators in a parallel application to reduce the input voltage from 24V to ±3.3V. Then I connect the positive output +3.3V from the switching regulator to LDO LP2992. The negative output of -3.3V with LDO TPS723. At +3.3V the switching regulator has the output current of 500mA and at -3.3V the output current is -400mA. The wiring of the switching regulator is shown below.
Can LP2992 and TPS723 withstand these currents from the switching regulator?
What do I have to consider if I want to connect a switching regulator with linear regulators?
Kind Regards
Selvedin Hodzic