Hi,
I'm looking for a Buck Boost regulator with Dual positive output. Below are the specification:
Input: 3.0V (2 Alkaline AA Batteries operated).
Outputs: 3V@1A and 1.8V@1mA
What could be the possible solution for NB-IoT applications with sensors that has different voltage level?
Most of the ICs (modules and sensors) in our design needs 3V supply, but one of the sensor needs 1.8V supply.
I'm thinking to have separate buck converter for the 1.8V sensor and boost converter for the rest of the ICs.
What could be the best solution?
Note: I'm using a level shifter TXS0102 for the I2C interface for the sensor (with 1.8V requirements), but I saw there is a buck converter with I2C interface. However, I'm not sure if it is applicable for my design.
Thank you.