hi,
we're using the bq76930 for a 20 cells battery system, now we meet some problems about the DEVICE_XREADY and need some help.
the system can working normal in the state without balance. and there is some abnormal event occurs when we do the cells balance.
in the charging time, we will set the cells balance on, some minutes later , DEVICE_XREADY is set to 1. if we stop the cells balance, and clear the DEVICE_XREADY, it will recover the normal state.
we do the balance at 2 cells Intervals, for example, the 2nd is balancing on, than the 3rd, 4th is off, and 5th is on(if the 5th cell voltage meet the balance voltage).
thank you.