This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2491: Solenoid output

Part Number: TPS2491

Not having all of the required information as yet, I have an application where I need to switch 32V max into either one or two solenoids in parallel.  I do not know the inductance value (working on that), but I've been told that the nominal resistance would be 18.5 Ohms which translates to 1.75 Amps.  The worse case current is supposed to be less than 2 Amps per solenoid.  However, the customer believes that the inrush current will be somewhere between 8 to 10 Amps per solenoid.  Like the inductance, I am trying to find out the duration of that inrush.

Would the TPS2491 be a good fit for this application?  If so, would excel spreadsheet be useful to use?