Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO,
Hi,
I have some questions.
I want to get your kind reply about my inquiry.
* Our customer's configuration for fuel gauge.
We use default except below items.
ChemID: 0x1202
Design capacity: 80mAh
Design energy: 296mWh
Terminate voltage: 3400mV
Taper rate: 384
Sleep current: 1mAh
Q invalid MaxV: 3800mV
Q invalid MinV: 3700mV
V at chg term: 4200mV
Taper voltage: 4100mV
* Symptoms.
1. When reach a point between the 2-8% it suddenly jumps to 99% SoC and stays there.
2. some times, SoC is jumping.
3. When charging, SoC changed from 92% to 2%.
* Below is my questions.
1. How do I have to set which items of Data Memory to clear above symptoms?
2. When I testing Learning Cycle, error has occurred.
error message is inserting charger. at that time, during charging.
3. Could you send example file for setting Data Memory?
4. Could you explain and setting guide for Ra Tables?
5. How do I calibration?
Best regards,
Michael