Hi,
There was no reply on the following E2E.
https://e2e.ti.com/support/power-management/f/196/p/923171/3410743#3410743
Therefore, I would like to ask additional questions in a new thread.
1.
When the total CB time exceeds "CB:Delta Threshold", the PF alert bit becomes ”1”.
Is this understanding correct?
And Please tell me because the meaning of "Time Cell 1..4" is unclear.
2.
If 1. is correct, Where should I check the "total Time cell 1..4"?
The customer wants to test that the PFAlert bit is set when it exceeds the set "CB Delta Threshold" while comparing it with "total Time cell 1..4".
Best regards,
Yusuke