TI Team,
We have designed a universal input SMPS (PFC + LLC) with an output of 25VDC. It uses two UCC24612-2DBVR devices in the SR section. Our client's CM would like to power the +25VDC net during some of their tests without having to power up the SMPS. In this use case, a lab supply is connected to the +25VDC net and ground nets via test points as shown in the graphic below. Since the UCC24612 is connected to this net, I would like to confirm that there any risk to the the synchronous rectifier controller in this scenario.
Can you confirm?
Thanks in advance!