hello,
We use a LM2576HV-Adj IC for power supply. Cin 100uf/ Cout 330uf/ L 330uH/ Diode SK39A/ Vin 60V/ Vout 12V.
we used one switch for on/off the output voltage. we connect pin5 of LM (ON/OFF pin) with R 4.7K to Vin and with Switch to GND.
Applying 60V input:
When the switch is connected, pin 5 from the IC is connected to ground and we have 12V output voltage. By disconnecting the switch, the output voltage is zeroed correctly.
But:When we reconnect the switch; to have voltage at the output, a problem occurs and the IC burns out and also draws 1 amp from the input.
We have installed only one LED series a resistance of 10 kg for the output load.
What is our problem? Is 60V too high for the ON/OFF pin IC?
Thanks