This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5036: Connecting Two LED's parallel in a single channel

Part Number: LP5036
Other Parts Discussed in Thread: AFE4490, TPS92511, LP5024, LP5018

Hey Ti Support team,

We have a requirement to control slightly more number of LED's (~40 LED's) with LP5036. Is it possible to connect two LEDs in parallel to a single channel ? (We are okay to limit the brightness of the two LEDs by keeping the total channel current under limit and the we are okay with controlling two LED's with same channel pattern in LP5036). Keeping these requirement, is it possible to connect Two parallel LED's in same channel of LP5036 ?

With Regards,

Nithin M