This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Comp pin

Part Number: UCC28950


Hi,

It is written on the datasheet as below.

"The range of the error amplifier output of 0.25 V to 4.25 V far exceeds the PWM comparator input ramp-signal range, which is from 0.8 V to 2.8 V."

Does this mean that the error amplifier output should not exceed the range 0.8V to 2.8V?

Best Regards,

Kuramochi