This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61160: Operation mode (no use PWM input) and Duty cycle spec.

Part Number: TPS61160


Hi,

I have a question about TPS61160 LED driver. Condition is below.

- 4 LED: Not white LED, typ.1.6V Vf / 1 LED
- CTRL: connect to 3.0V_REG
- LED current: about 2 - 40 mA (typ. about 15mA)

In the datasheet, "Maximum duty cycle" is shown about 93%.

Is it case by just using PWM input?

We will not use the PWM input for adjust a LED current. We think a constant voltage input operation with TPS61160, it looks good operation. Therefore duty cycle is 100% in this case.

Best regards,

KoT