Hi all,
I have a question regarding this P/N: can I assume that, when EN pin is low (< Ven-VCC_h), the SW pin is “high impedance”?
I would need to understand if I can apply a voltage to it, without shorting out. I guess I can, since VCC regulator should be disabled so there’s no way that the low side output mosfet is on.
What I need to do, basically, is to short together the two outputs of LMR36520ADDAR-based buck converter (after the inductor, I mean) for a “redundant” power supply (one from +48V, one from 7.2V battery). Both are set for 3.3V output, and they are interlocked in the sense that they cannot be enabled simultaneously.
Thanks,
Oz