Hi Sir,
Can we set both precharge and termination current = 60mA?
There is 60mA offset for precharge and termination current already, so we just need to set REG03 = 00h, right?
Thank you.
Regards,
Allen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Can we set both precharge and termination current = 60mA?
There is 60mA offset for precharge and termination current already, so we just need to set REG03 = 00h, right?
Thank you.
Regards,
Allen
Allen,
It should be ok. The charger device automatically terminates the charging cycle when the charging current is below termination threshold, battery voltage is above recharge threshold, and device not is in DPM mode or thermal regulation.
Thanks,
Ning.