Hello, I've got a design on which I'm trying to stabilize the voltage on a very sensitive (to ripple) module. The module would normally receive 5.17V and the ripple is constrained at max 35mVpp. Occasionally the input drops or has higher ripple so I've decided to insert TPS63050RMWR chip to keep the 5.17V under control but I am worried that at Vin Voltages close to the Vout, the Vout may not be stable enough even though the datasheet says "seamless transition between buck and boost. I simulated this in WeBench and it appears to work based on my input data and simulation results but des anyone has real life experience with tis type of configuration or can anyone comment if this would be the right chip to use? The current is max 0.5A