Other Parts Discussed in Thread: UCD90120
Hi All,
I am facing problems while reprogramming UCD90120 on ZC706.
I have Rev 2.0 for ZC706 and initially, I followed this link to download the XML files:
https://www.xilinx.com/support/answers/53599.html
I made a mistake of misunderstanding the statement "ZC706 Rev 1.0 and beyond" and used ZC706_Rev1_XML.zip file to reprogram my rev 2.0 board. On TI Digital Power Manufacturing Tool I got this error while programming: "READ_OUT on rail#1(0.001V) was not within 5% of VOUT_COMMAND(1.000V)"
While looking at forums for solution I realized that there is a separate XML file for Rev 2.0. So I downloaded that file from https://www.xilinx.com/support/answers/64890.html
In addition, I upgraded the TI programmer firmware as I read that can cause issues as well.
After I cleared the previous configuration and reprogrammed UCD90120, finally it was successful which gave me a bit of relief
But the issue was most of the power LEDs were still not ON and the FPGA chip was getting pretty hot.
I used TI Fusion digital power designer to perform power monitoring and this is what I can see:
The Rail#1 (VCCINT) is showing correct Vout (1 V) but Iout is too high and I am getting Over voltage warning. I am assuming that is the reason why remaining rails are not giving any output but I am not sure.
I am not sure what is happening here. I used the correct XML file now and reprogramming was also successful. Kindly help me out here. What can be the reason behind this?
Thanks in advance
Regards