This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5145: Quick high and low enable control

Part Number: LM5145

Hi sir,

Can we control LM5145RGYR enable pin for high with 5msec and low with 1sec, then cycling? Will LM5145RGYR broken?

Below is our application, when the loading current is 30mA,will power off LM5145 and power device by other source; if the load current is 200mA, power on LM5145, but the time duration is only 5msec. The frequently switch on/off LM5145 might has transient issue?

#Note: Vin of LM5145 is 12V/ 24V/ 48V; Vout is 5V

Thanks!

Hedy