This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: Current from output to input

Part Number: TPS61022

Hi team,

My customer intend to use TPS61022 as a backup power supply. Input of the TPS61022 is connected to a primary battery. The TPS61022 is usually disabled and there is voltage about 5V on the output from an external power source. We want to be sure that there is no current flow from the output to the input when TPS61022 is disabled.

Can you please confirm that the input is disconnected from the output when the device is disabled?

What is the leakage current flow from OUT pin to SW pin when TPS61022 disabled?