I am using TPS65910 with AM3715. A SD card attached to MMC interface of AM3715 will be used as booting source. As the reference design, the MMC/SD interface of AM3715 and the SD card are powered from VMMC rail of TPS65910. However VMMC is default to OFF when it is in AM3715 setting mode (BOOT0/1=10). It means that both MMC/SD interface of AM3715 and the SD card will have no power until TPS65910 is initialized. But the initialization code of the PMIC is located in SD card. So we are in a died loop.
The solution seems to power MMC/SD interface and SD card from a default ON rail, any suggestions about which rail we should use? Only SD card will be used so what we need is a default ON 3.3V rail with at least 150mA capacity.
thanks
Jiansheng