My customer is using LP8860-Q1 (D version) applied to AVN.
There is currently a product with a problem with changing EEPROM Setting Data.
LP8860-Q1 (Dversion) According to the application, there is no problem with mass production products, but there is a problem while considering applying it to the new model.
attachments will be modified EEPROM Read value.
A customer writes an EEPROM at the first start, and rewrites the EEPROM when the read value becomes a problem.
I think it's been over 1000 cycles since I started rewriting without EEPROM lock.
The following questions need to be checked.
1. The customer will change it to 0xFA (the default value of 0xF8 of type D) at 0x66 and save it to the EEPROM.
However, is the behavior changed if the 0x66 value is sent every time without writing to the EEPROM?
The action I want is to write 10 on BRT_MODE.
2. What causes the EEPROM Register value to change when the data is not written after EEPROM_UNLOCK?
3. Is there a way to check the number of EEPROM writes?