Part Number: LP8555
Hi,
The datasheet that there is a soft-start function in LP8555 section 8.3.1.1.
What are the specifications about this soft-start function?
With an inductance 10uH I measure a peak inductance current during start-up at 1.5A and a rising time of Boost output voltage at 100us.
Have you recommendation to reduce this peak current?
Vin= 5,25V
VOUT=VINIT= 14.45V
Thanks in advance.
Regards,
Kouassi KRA